Hydrogen fuel cell systems
Fully optimized and integrated solution, suitable for prime energy, peak shaving, and emergency backup power applications, converting hydrogen to electricty with water vapor as the primary by-product at the point of use.
Putting resilience at the heart of sustainability
Creating value with innovative, sustainable solutions.
How Powering Impact™ comes to life at Rehlko.
Discover the full spectrum of Rehlko sustainable power solutions for data centers.
Built for speed. Ready for what's next.
Fully optimized and integrated solution, suitable for prime energy, peak shaving, and emergency backup power applications, converting hydrogen to electricty with water vapor as the primary by-product at the point of use.
Advanced life-cycle care and maintenance program for KD Series™ generators allows customers to reduce costs and emissions depending on use and configuration of the system.
All Rehlko diesel engines and power generators are HVO fuel compatible which allows users to further decrease the carbon footprint across a generator's lifecycle.
Rehlko offers tailored biogas upgrading systems that clean biogas (CH4 and CO2) into concentrated streams of renewable natural gas and carbon dioxide (bioCO2). RNG can be used to defossilize gas grids and act as a sustainable transportation fuel.
Combined cooling, heat, and power (CCHP) systems anchored in gas engines, produce electricity, heat and or cooling. In certain CCHP applications, overall system efficiency can approach 90% by capturing and utilizing thermal energy that would otherwise be wasted, increasing the amount of energy used from the same fuel.
Helps data center customers manage highly variable utility rate structures, load spikes with high-demand charges, and grid instability by balancing energy supply and demand behind-the-meter or as part of a hybrid system.
The Rehlko Power Impact Intelligence is a strategic platform that can give data center operators direct, decision ready insight into the carbon impact of their power systems. Unlike static reports or disconnected data sources, it can deliver clear insight to support more informed infrastructure choices, including those that may reduce carbon emissions.
Creating an energy resilient world for a better future.
Guided by our purpose—creating an energy resilient world for a better future—we continue to reduce reliance on the grid by advancing cleaner, more sustainable energy solutions that provide continuity, confidence, and long-term impact.
How powering impact comes to life at Rehlko
We embed our sustainability strategy across three main pillars of impact:
Our integrated suite of innovative, sustainable solutions allows our customers to more progressively meet their sustainability goals.
Our operational model is designed for our processes and products to be sustainable from the inside out.
We invest time and resources to support our team members and the places they call home.
Our goal:
How Rehlko is working to build the foundation for a stronger, sustainable future.
Rehlko is helping shape a more sustainable data center industry through its leadership in the iMasons Climate Accord. Working alongside global partners across equipment, materials, power, and water, Rehlko is advancing practical solutions to decarbonize digital infrastructure. With leadership roles in key working groups and contributions to industry frameworks and reports, Rehlko is turning collaboration into measurable climate progress.
In 2025, we reduced Scope 1 and 2 emissions by 19.6%, diverted 81.2% of waste from landfill, and achieved 100% scrap metal recycling—advancing performance across our operational footprint.
Clarke's Nigeria operations are advancing cleaner, more sustainable practices through waste reduction initiatives, energy-efficiency upgrades, and the transition to lower-emission equipment across their facilities.
A fully integrated clean energy storage and distribution system at Rehlko’s France facility has already reused more than 6,500 kWh of energy and reduced 12 MT CO2e, showcasing scalable, smart energy solutions that support customers’ energy transition goals.
Rehlko’s France facility is advancing circular economy practices through innovative material reuse, recycled logistics solutions, and partnerships that extend the life of equipment and reduce waste.
That's the value of powering impact.
Together we are working to simultaneously scale our businesses while addressing specific sustainability challenges.
We continue to focus on delivering innovative solutions to support our customers who seek rapid, reliable, and resilient power. Our projects combine our engineering excellence with our purpose: creating an energy resilient world for a better future.